SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The enhanced peripheral interrupt expander (ePIE) module is used to interface peripheral interrupts to the C28x CPU. The ePIE module provides configurable masking on a per interrupt basis. The ePIE module includes a local SRAM that is used to hold the address of the interrupt handler per interrupt.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):
The following tests can be applied as a test-for-diagnostic on this module: