SFFS889 July 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
ePWM modules can be chained together through a clock synchronization scheme that allows the the ePWM modules to operate as a single system when required. In the synchronous mode of operation, checking the proper synchronization of the various PWM instances is critical to avoid catastrophic conditions. The synchronization of the various PWMs can be checked by reading the TBSTS.SYNCI bit of the ePWM module. The proper phase relationship intended as a result of the sync operation can be cross-checked by comparing the TBCTR register value.