SFFS911 December   2024 TMAG5110-Q1 , TMAG5111-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 TMAG5110-Q1
    2. 2.2 TMAG5111-Q1
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 TMAG5110-Q1
    2. 4.2 TMAG5111-Q1
  7. 5Revision History

TMAG5110-Q1

Figure 4-1 shows the TMAG5110-Q1 pin diagram for the DBV package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TMAG5110-Q1 data sheet.

TMAG511x-Q1 TMAG5110-Q1 TMAG5111-Q1 Pin Diagram
                                        DBV Package Figure 4-1 Pin Diagram DBV Package
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VCC1A lot of current can be sourced external to the device, with the current only limited by the source that supplies VCC and the total resistance between the supply and ground. Depending on the layout, a short can conduct enough heat to damage the part.B or A
GND2Normal, recommended operation.D
NC3Normal, recommended operation.D
OUT14OUT1 is always low, current is limited and heat dissipation is limited by the external pull-up resistor.B
OUT25OUT2 is always low, current is limited and heat dissipation is limited by the external pull-up resistor.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VCC1Device is unresponsive but not damagedB
GND2Device is not functional and not damaged.B
NC3Normal operation.D
OUT14Device output is disconnected from the system. Device is not damaged, functionality within the system is lost until open fixed.B
OUT25Device output is disconnected from the system. Device is not damaged, functionality within the system is lost until open fixed.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
VCC1GNDA lot of current can be sourced external to the device, with the current only limited by the source that supplies VCC and the total resistance between the supply and ground. Depending on the layout, a short can conduct enough heat to damage the part.B or A
GND2NCNormal, recommended operation.D
NC3OUT1Functional and not damaged, however, not recommended.D
OUT14OUT2Erroneous output. OUT1 and OUT2 are dominated by whichever is in the low state. Functionality is lost and increased consumption of current is possible.B
OUT25VCCDevice OUT2 is stuck high, the worst-case current is only limited by output drain RDS(on). If on sufficiently long, the output can be damaged.B or A
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCC
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
VCC1Normal OperationD
GND2A lot of current can be sourced external to the device, with the current only limited by the source that supplies VCC and the total resistance between the supply and ground. Depending on the layout, a short can conduct enough heat to damage the part.B or A
NC3Not recommended, however, the part is expected to maintain functionality and not be damaged.D
OUT14Device OUT1 is stuck high, the worst-case current is only limited by output drain RDS(on). If on sufficiently long, the output can be damaged.B or A
OUT25Device OUT2 is stuck high, the worst-case current is only limited by output drain RDS(on). If on sufficiently long, the output can be damaged.B or A