SFFS944 July   2024 TPS3703

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS3703. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to VDD (see Table 4-5)
  • Pin short-circuited to /RESET is also included (see Table 4-6)

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality.
B No device damage, but loss of functionality.
C No device damage, but performance degradation.
D No device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS3703 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS3703 data sheet.

TPS3703 Pin DiagramDSE Package6-Pin WSON Figure 4-1 Pin DiagramDSE Package6-Pin WSON

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • VDD = 3.3V, V_SENSE = 1.2V, /RESET pulled-up to VDD unless stated otherwise
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SENSE 1 No damage to device, can affect application functionality. Shorts voltage supply to ground, increases current. C
VDD 2 No damage to device, can affect application functionality. Shorts voltage supply to ground, increases current. C
CT 3 Normal operation, device in latch mode. Usually has pull-down resistance to limit currEnt. D
/RESET 4 No damage to device, can affect application functionality. Forces /reset to be asserted. C
GND 5 Normal operation. D
/MR 6 Normal operation in some cases, but forces /reset to be asserted. C
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SENSE 1 No damage to device, can affect application functionality. /Reset tends to be low. C
VDD 2 No damage to device, but device is not powered. /Reset tends to be low. C
CT 3 Normal operation. D
/RESET 4 Open drain output requires pull-up voltage for functionality. C
GND 5 No damage to device, but device is not powered. /Reset tends to be low. C
/MR 6 Normal operation. Pin is internally pulled up to VDD. D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
SENSE 1 VDD Normal operation in some applications. Functionality affected with separate supply for sense, but no damage. C
VDD 2 CT Normal operation. Usually has pull-up resistance to limit current. D
CT 3 /RESET No damage to device, but device is not powered. /Reset tends to be low. C
/RESET 4 GND No damage to device, can affect application functionality. Forces /reset to be asserted. C
GND 5 /MR Normal operation in some cases, but forces /reset to be asserted. C
/MR 6 SENSE Undefined operation, but functionality can be affected. When MR is asserted, SENSE shorts to GND. C
Table 4-5 Pin FMA for Device Pins Short-Circuited to VDD
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SENSE 1 Normal operation in some applications. Functionality affected with separate supply for sense, but no damage. C
VDD 2 Normal operation. D
CT 3 Normal operation. Usually has pull-up resistance to limit current. D
/RESET 4 Normal operation. Usually has pull-up resistance to limit current. D
GND 5 No damage to device, can affect application functionality. Shorts voltage supply to ground, increases current. C
/MR 6 Normal operation, but increased leakage current. Internally pulled-up to VDD to limit current. D
Table 4-6 Pin FMA for Device Pins Short-Circuited to /RESET
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
SENSE 1 No damage to device, can affect application functionality. Forces /reset to equal sense voltage. C
VDD 2 Normal operation. Usually has pull-up resistance to limit current. D
CT 3 No damage to device, can affect application functionality. /Reset tends to be low. C
/RESET 4 Normal operation. D
GND 5 No damage to device, can affect application functionality. Forces /reset to be asserted. C
/MR 6 No damage to device, can affect application functionality. Forces /RESET to latch. C