SFFS953 December 2024 TCAN1043N-Q1 , TCAN1473-Q1
This section provides a failure mode analysis (FMA) for the pins of the TCAN1043N-Q1 and TCAN1473-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-7 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the SOIC (D) pin diagram. Figure 4-2 shows the VSON (DMT) pin diagram. Figure 4-3 shows the SOT (DYY) pin diagram.
For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TCAN1043N-Q1 and TCAN1473-Q1 data sheets.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
TXD | 1 | TXD biased dominant indefinitely. The device enters dominant time-out mode. Unable to transmit data. | B |
GND | 2 | None. | D |
VCC | 3 | Device enters Sleep mode. There is a high current draw from the external regulator that supplies to the VCC pin. | B |
RXD | 4 | Receiver output biased recessive indefinitely. The host is unable to receive data from the bus. | B |
VIO | 5 | Device enters Sleep mode. Transceiver is passive on bus. There is a high current draw from the external regulator that supplies to VIO. | B |
EN | 6 | EN pin biased low. The device is not able to enter normal mode. Unable to communicate. | B |
INH | 7 | High ISUP current, the INH pin can be damaged and indication from sleep mode transition is not available. | A |
nFAULT | 8 | nFAULT pin biased low indefinitely, which indicates a fault indefinitely. | B |
WAKE | 9 | WAKE pin biased low indefinitely and is not able to utilize the local wake-up function. | B |
VSUP | 10 | Device is not powered. There will be a high current flowing from the source supplying to the VSUP pin (battery) to the ground. | B |
NC | 11 | None. | D |
CANL | 12 | VO(REC) specification is violated, degraded EMC performance. | C |
CANH | 13 | Device cannot drive dominant bit to the bus, no communication possible. | B |
nSTB | 14 | nSTB biased low indefinitely. The transceiver is unable to enter normal mode. Unable to communicate. | B |
Thermal Pad | - | None. | D |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
TXD | 1 | TXD pin defaults to a recessive bias. The device is always recessive and unable to transmit data. | B |
GND | 2 | Device is not powered. | B |
VCC | 3 | Device is in protected mode. | B |
RXD | 4 | No RXD output, unable to receive data. | B |
VIO | 5 | Device is in protected mode. | B |
EN | 6 | EN pin defaults to a logic-low bias. The device is not able to enter normal mode. Unable to communicate. | B |
INH | 7 | None. | D |
nFAULT | 8 | No effect on the device performance, unable to monitor system faults. | B |
WAKE | 9 | No effect on the device performance, unable to use the local wake-up function. | B |
VSUP | 10 | Device is not powered. | B |
NC | 11 | None. | D |
CANL | 12 | Device cannot drive dominant on bus and is unable to communicate. | B |
CANH | 13 | Device cannot drive dominant on bus and is unable to communicate. | B |
nSTB | 14 | nSTB defaults to a logic-low bias. The device is not able to enter normal mode. Unable to communicate. | B |
Thermal Pad | - | None. | D |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
TXD | 1 | GND | TXD is biased dominant indefinitely. The device enters dominant time-out mode. Unable to transmit data. | B |
GND | 2 | VCC | Device is in protected mode, high ICC current. | B |
VCC | 3 | RXD | RXD output biased recessive indefinitely. The controller is unable to receive data from CAN bus. | B |
RXD | 4 | VIO | RXD output biased recessive indefinitely. The controller is unable to receive data from CAN bus. | B |
VIO | 5 | EN | EN pin biased high indefinitely. The device is unable to enter standby and silent mode. | B |
EN | 6 | INH | Absolute maximum violation on the EN pin, except in sleep mode. Transceiver can be damaged. | A |
nFAULT | 8 | WAKE | Potential absolute maximum violation on nFAULT pin if WAKE is biased high. Transceiver can be damaged. | A |
WAKE | 9 | VSUP | WAKE biased high indefinitely, unable to utilize the local wake-up function. | B |
VSUP | 10 | NC | None. | D |
NC | 11 | CANL | None. | D |
CANL | 12 | CANH | Bus biased recessive. No communication is possible. IOS current can be reached on CANH/CANL. | B |
CANH | 13 | nSTB | Driver and receiver turn off when the CAN bus is recessive. Potentially does not enter normal mode. | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
TXD | 1 | TXD biased recessive indefinitely, unable to transmit data. | B |
GND | 2 | CAN transmitter is not powered and the device enters Sleep mode. There is a high current draw from the external regulator supplying to the VCC pin. | B |
VCC | 3 | None. | D |
RXD | 4 | Receiver output biased recessive indefinitely. Host is unable to receive data from bus. | B |
VIO | 5 | I/O pins operate as 5V inputs and outputs. Microcontroller can be damaged if VCC > VIO. | C |
EN | 6 | EN biased high indefinitely. The device is unable to enter standby and silent mode. | B |
INH | 7 | Absolute maximum violation on VCC pin. INH is biased at VCC voltage. System potentially does not wake up. | A |
nFAULT | 8 | nFAULT biased high indefinitely. The transceiver is unable to report faults. | B |
WAKE | 9 | None. | D |
VSUP | 10 | Absolute maximum violation on VCC. | A |
NC | 11 | None. | D |
CANL | 12 | IOS current can be reached, RXD is always recessive. | B |
CANH | 13 | VO(REC) specification is violated, degraded EMC performance. | C |
nSTB | 14 | nSTB biased high indefinitely. The transceiver is unable to enter standby and sleep mode. | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
TXD | 1 | Absolute maximum violation, transceiver can be damaged. | A |
GND | 2 | Device is not powered, high ISUP current. | B |
VCC | 3 | Absolute maximum violation, transceiver can be damaged. | A |
RXD | 4 | Absolute maximum violation, transceiver can be damaged. | A |
VIO | 5 | Absolute maximum violation, transceiver can be damaged. | A |
EN | 6 | Absolute maximum violation, transceiver can be damaged. | A |
INH | 7 | Minimal current driven into the INH pin. | D |
nFAULT | 8 | Absolute maximum violation, transceiver can be damaged. | A |
WAKE | 9 | WAKE biased high, unable to use the local wake-up function. | B |
VSUP | 10 | None. | D |
NC | 11 | None. | D |
CANL | 12 | IOS current can be reached. RXD is always recessive. | B |
CANH | 13 | VO(REC) specification is violated, degraded EMC performance and communication errors can also result. | C |
nSTB | 14 | Absolute maximum violation, transceiver can be damaged. | A |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
TXD | 1 | TXD biased recessive indefinitely, unable to transmit data. | B |
GND | 2 | Device is not powered. There is a high current draw from the external regulator supplying to the VIO pin. | B |
VCC | 3 | I/O pins operate as 5V inputs and outputs. Microcontroller can be damaged if VCC > VIO. | C |
RXD | 4 | Receiver output biased recessive indefinitely. Host is unable to receive data from bus. | B |
VIO | 5 | None. | D |
EN | 6 | EN biased high indefinitely. The device is unable to enter standby and silent mode. | B |
INH | 7 | Absolute maximum violation on the VIO pin. INH is biased at VIO voltage. System potentially does not wake up. | A |
nFAULT | 8 | nFAULT biased high indefinitely. The transceiver is unable to report faults. | B |
WAKE | 9 | None. | D |
VSUP | 10 | Absolute maximum violation on VIO. | A |
NC | 11 | None. | D |
CANL | 12 | IOS current can be reached, RXD is always recessive. | B |
CANH | 13 | VO(REC) specification is violated, degraded EMC performance. | C |
nSTB | 14 | nSTB biased high indefinitely. The transceiver is unable to enter standby and sleep mode. | B |