The TLC3544 and TLC3548 14-bit serial-output analog-to-digital converters can easily interface to the serial peripheral interface port of many popular microcontrollers. Using the serial port of the TI MSP430F149 MCU, this application report focuses on configuring, sampling, and converting analog data presented to the ADC. The assembly code developed for this application report shows how the EOC/INT pin can be used as an interrupt source to the host processor.
The associated source code is available from http://www.ti.com/lit/zip/slaa126.
MSP430 is a trademark of Texas Instruments.
All other trademarks are the property of their respective owners.