SLAA126B April 2001 – September 2018 MSP430F149 , MSP430F149 , TLC3544 , TLC3544 , TLC3548 , TLC3548
The FS input signal is normally used in DSP based systems to indicate the start of a serial data frame. If FS is low at the falling edge of CS, the rising edge of the frame sync pulse initiates the sample-and-convert cycle. FS should be pulled to DVDD when not in use.
The TLC3544/48 evaluation module uses a common frame-sync line for both the ADC and DAC. The Xilinx PLD located at U15, acts as a gatekeeper by determining which device (ADC or DAC) should receive the incoming signal. When the HOST_CNTLa line is low (ADC is selected), the PLD routes the incoming FS to the ADC. When HOST_CNTLa is high, the FS signal is applied to the DAC.