SLAA450G April 2010 – April 2020
To run the demo, connect the LaunchPad to the host PC. This power the board, allows downloading of code through Spy-Bi-Wire for the debugging purposes, and (most important for BSL operation) provides a UART interface, as every onboard emulation circuit of the LaunchPad comes with a free Application UART. The Application UART is used to provide a USB-to-UART bridge to the host PC.
NOTE
Any other way of providing a UART interface to the device also works, as long as voltage and timing requirements are met.