SLAA450G April 2010 – April 2020
Development of the customer application happens as always by creating specification, coding, debugging, and testing. There is no need to include the BSL in the project at this point.
For convenience, two project demos are available, in C and Assembler, that can be used as a starting point for application development (see Section 2.3 for details).
NOTE
Information memory cannot be used for user code. It is good practice to uncheck 'erase Info memory' in the debug options, so that this area cannot be used by accident.