SLAA534A June 2013 – June 2020
The MSP430's exception handling table format and mechanism is based on that of the ARM processor family, which itself is based on the IA-64 Exception Handling ABI (http://www.codesourcery.com/public/cxx-abi/abi-eh.html). This section focuses on the MSP430-specific portions.
TDEH data consists of three main components: the EXIDX, the EXTAB, and catch and cleanup blocks.
The Exception Index Table (EXIDX) maps program addresses to entries in the Exception Action Table (EXTAB). All addresses in the program are covered by the EXIDX.
The EXTAB encodes instructions which describe how to unwind a stack frame (by restoring registers and adjusting the stack pointer) and which catch and cleanup blocks to invoke when an exception is propagated.
Catch and cleanup blocks (collectively known as landing pads) are code fragments that perform exception handling tasks. Cleanup blocks contain calls to destructor functions. Catch blocks implement catch clauses in the user's code. These blocks are only executed when an exception actually gets thrown. These blocks are generated for a function when the rest of the function is generated, and execute in the same stack frame as the function, but may be placed in a different section.