SLAA534A June 2013 – June 2020
The R_MSP430_NONE relocation type performs no operation. It is used to create a reference from one section to another, to ensure that if the referring section is linked in, so is the referent section.
R_MSP430_PREL31 is used to encode code addresses in exception handling tables. See Section 9.3.
R_MSP430_EHTYPE is used to encode typeinfo addresses in exception handling tables. See Section 9.7.1.