SLAA638A august 2014 – may 2023 MSP430I2040 , MSP430I2041
A set of calibration factors that gives reading roughly to an accuracy of a few percent is defined in the example code. If more accurate result is preferred, the EVM needs to undergo a process of calibration. For more information on the calibration procedure, see Section 3. The following list of instruments are suggested in order to perform calibration:
The links below are the links to the instrument used for testing and calibrating the design:
AC Source: http://www.chromausa.com/acpowersources/61500lo-ac-source.php
Reference Meter: http://www.chromausa.com/powermeters/66201-66202-digital-power-meters.php
DC Electronic Load: http://www.chromausa.com/dcloads.php#6310a