SLAA638A august 2014 – may 2023 MSP430I2040 , MSP430I2041
The design of the EVM allows that the DC measurement parameters be calibrated automatically, the same time that AC is being calibrated. In the last step of calibration (current AC offset), the DC measurement parameters are automatically updated.
In fact, whenever the complete set of calibration value is read, the most update DC measurement parameters are also included in the set. When an update is done to the other parameters, the DC measurement parameter is also updated to the most updated value. However, the value is most accurate when the current is low (best with no current at all), thus, it is suggested to perform the DC measurement parameter update after the I_AC_OFFSET calibration.
This may not be a user friendly way of setting DC measurement parameters. The procedure of having the best DC measurement parameters is modified and improved when the embedded metering customized calibration software is released.