SLAA721E October 2016 – March 2020 MSP430FR5969 , MSP430FR5969-SP , MSP430FR5994 , MSP430FR6989
This software package includes examples for the MSP430FR5969, MSP430FR5994, and MSP430FR2433 on their LaunchPad™ development kits (MSP-EXP430FR5969, MSP-EXP430FR5994, and MSP-EXP430FR2433, respectively) (see Figure 4-1).
The bootloader and demo applications use the same LED (LED1 and LED2) and push button (S1 and S2) notations across all variants of the LaunchPad development kits. The pin assignments that correspond to these I/O peripherals are different for each board derivative. For ease of use, the examples have been designed so that the host and target LaunchPad development kits should be the same derivative, although this can be modified for different configurations if desired.