SLAA843A August 2018 – March 2019 MSP430FR2512 , MSP430FR2512 , MSP430FR2522 , MSP430FR2522 , MSP430FR2532 , MSP430FR2532 , MSP430FR2533 , MSP430FR2533 , MSP430FR2632 , MSP430FR2632 , MSP430FR2633 , MSP430FR2633
Robustness refers to the ability of a system to operate as intended even when it is not used within the specified operating conditions. For example, a product is reliable if it operates correctly within its expected temperature range. However, the product may be considered reliable and robust if the product operates correctly even when it is outside of the expected temperature range. Likewise, a capacitive touch interface could be considered robust if it operates correctly in a residential environment for which it was designed, but it also operates correctly in a harsher commercial or industrial environment for which it was not designed. This is an important distinction for capacitive touch interfaces for two reasons: