Constant voltage audio systems are commonly used in installations where audio information needs to be distributed over long and varied distances to many different points of load with high total power delivery. These systems are widely used in commercial building installations for public announcement (PA) or for fire safety and building security notifications by specific zone. This application note describes the operation of constant voltage audio systems and derives the equations needed to determine overall system efficiency. Advantages of integrated power amplifiers, such as the TPA3255, compared to traditional discrete amplifier implementations are discussed. An example system was built using the TPA3255 and measurements were taken with different audio transformers to show the impact that different transformer parameters have on overall system efficiency.
Peavey® is a registered trademark of Peavey Electronics Corp.
EDCOR® is a registered trademark of EDCOR Electronics Corporation .
All trademarks are the property of their respective owners.
Constant voltage audio systems are used to distribute audio over large areas. Whether in an airport terminal PA system or fire safety notification systems, constant voltage audio systems ensure that the audio is effectively distributed to speakers around the facility. To achieve such widespread audio distribution, power amplifiers are needed within the system to drive the distributed speaker network. Each amplifier can then be controlled to send the same or different sounds, depending on the zone. An example of a sound that would be the same throughout a system is music in a shopping mall. An example of a sound that would be different, depending on the zone, is different evacuation messages for different floors in a multi-story building. Regardless of use, the power amplifier stage of the constant voltage audio system plays a crucial role. Though that has traditionally been achieved through discrete implementation, it can be done with integrated Class-D amplifiers, typically at lower cost and in a smaller area.