Speaker parameters can vary from the vendor
datasheet with a tolerance, and each speaker may vary from each other as well. This can
lead to inaccurate speaker protection when one speaker model is used to fit all
speakers. For this reason TI’s Smart Amp algorithms can be calibrated accordingly to
each speaker variance to ensure proper and accurate function of speaker protection. The
FTC is performed to calibrate the Smart Amp algorithm and protect the speaker from
parameter variations. The FTC obtains the speaker Re, f0, Q, and voice
coil temperature as seen below in step three of FTC Process shown below.
These parameters are then compared against pass/fail limits defined by the
customer in Step 4. Speakers that pass the parameter limits test will be configured with
new calibrated model as seen in the last step of
Figure 2-1. TI recommends to perform FTC on all units in order to ensure proper
protection of each speaker unit. For information on how to implement the FTC in your
system please refer to the
TAS2555, TAS2557, and TAS2559 Factory Test and Calibration
Guide.
Figure 2-2 contains all of the parameters the calibration test can measure
during each test. By setting the range of tolerable pass/fail limits, users can
determine if the speakers under testing are suitable for the system.