As shown in Figure 4-1, it shows the connection structure of the SAC inside FR235x.
- SAC0 as a TIA
- SAC2 as the gain stage
- ADC will capture SAC0 and SAC2
output
- SAC1 and SAC3 use to drive IR and RED
LED.
From the structure in Figure 4-1, you can get the voltage of SAC0 output (Vo1):
Equation 3. 
The voltage of SAC2 output (Vo2):
Equation 4. 
In order to improve the SNR of the
analog-to-digital converter (ADC) signal, the output signal of SAC2 needs to be adjusted
at ADC VREF/2. Therefore, the value of DAC2 needs to be adjusted in real time according
to the output of SAC0.
Equation 5. 
In the schematic (Figure 4-2), you can find that:
- Two SACs are used with transistors to
drive RED*IR LEDs
- SAC0+SAC2 are connected internally to
amplify photodiode signal
- A button is used to wake up the
system and start to measure
- A SPI interface is used to drive the
organic light-emitting diode (OLED) screen (include driver)
- An SBW and BSL inter-integrated
circuit (I2C) mode program debugging port
- An universal asynchronous
receiver/transmitter (UART) serial port used to communicate with GUI