Use a complete ground plane and a
complete power plane to avoid noise coupling. But in most cases, split ground
planes cannot be avoided. If split ground planes are essential:
Do not route signals over
a gap. Always strive for the return current flow with the smallest loop
area.
Connect split ground
planes only at one point. More common-ground connections can create
ground loops, and this increases radiation.
Power planes should only
reference their own ground plane. They should not overlap with another
ground plane.
Do not connect bypass
capacitors between a power plane and an unrelated ground plane. Again,
noise can be coupled from one supply system into the other.
Separate digital and analog power supplies with filtering and bypassing.
Put the largest-value filter
capacitors near a power connector and supply inputs.
Place high-quality X7R decoupling capacitors close to device pins.
Use multiple capacitors
(0.1 μF, 0.01 μF, and 1 μF) in parallel to offer low impedance over
higher frequency ranges.
Place the smallest-value
capacitors closest to the power pin.
Connect the pad of the
capacitor directly to a via to the ground plane. Use two or three vias
to get a low-impedance connection to ground.
Keep the traces from
decoupling caps to ground as short and wide as possible
Figure 2-6 Poor and Good Placement and
Routing of Bypass Capacitors