SLAAE47A May 2022 – August 2022 DAC11001A , DAC11001B
Load regulation is the measure of the variation in VREF as a function of load current and is specified either as a percentage or in parts-per-million (ppm) per milliampere (ppm/mA). It is calculated by dividing the relative change in VREF at minimum and maximum load currents by the range of the load current. Load regulation depends on both the design of the reference and the parasitic resistance separating it from the load, so the reference should be placed as close to the load as the PCB layout will allow.