SLAAEC6A October 2023 – January 2024
As shown in the figure below, the GPIO function and interrupt behavior can be configured in this tab. There are two General Purpose Inputs (GPI1 and GPI2), one General Purpose Output (GPO1), and one General Purpose Input Output (GPIO1) in the TAx5x1x-Q1 devices. These general-purpose input/output drivers also provide several multiplexing functions, and the selection can also be configured in this tab. Depending on the selection, some controls are grayed out. On the right side is the Interrupt selection, which has the settings as well as flag update/status of the respective interrupt.