SLAAED0 March 2024 TAS2764 , TAS2780 , TAS2781
For the click and pop measurement, only the Filtered Waveform section is important. You can discard the Averaging Mode, Averaging Time, and Averaged Data sections as these are not relevant to the click and pop measurement. Please make sure to choose A-weighting as Filter option in the window. This applies the A-Weighting filter on the Original Waveform and the resulted A-Weighted Waveform appears in the Filtered Waveform section. In Figure 6-14, zoom in around the Maximum peak level, and analyze both the original and A-weighted waveform outputs.
The original waveform is displaying a max peak level of approximately 1.4mV (similar to the capture in Measurement Recorder Window Output). At the same instance, the A-weighted filtered waveform displays a max peak level of approximately 1.1mV.