Determine the desired time
interval between each rail at start-up. The time interval set is counted
sequentially from rail to rail not the start point. See Design Considerations for instructions on calculating the
intervals.
Determine the desired time
interval between each rail at shutdown. The time interval set is counted
sequentially from rail to rail not the start point. Alternatively,
outputs can be shutdown all at once.
Configure peripherals in
SysConfig. Select a timer, configure with a chosen frequency, and set interrupt
as a zero event. Set the input interrupt as rising and falling edge. Choose pins
for input voltage and output rails.
Modify the desired time intervals
in the application code. Time intervals are place at the top of the
.c file.