Sample Rate Converters (SRC) are used whenever there is a need to convert an input sampling frequency to a different sampling rate. This application note introduces the TAX5X1X Synchronous SRC (SSRC), the supported sampling ratios, the different modes and follow by some use case examples.
SSRC is supported in TAC5212, TAC5211,TAC5112, TAC5111, TAD5212, TAD5112, and TAA5212 devices.
All trademarks are the property of their respective owners.