SLAAEI7 December   2023 MSPM0G3507

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Technology
    1. 2.1 Analog Peripherals in the MSPM0
    2. 2.2 Instrumentation Amplifier - INA350
    3. 2.3 Voltage Reference - REF2925
    4. 2.4 Low-Dropout Regulator - TPS7B6933-Q1
  6. 3Signal Chain
  7. 4Results
    1. 4.1 Influence of the OPA Chopping Mode
    2. 4.2 Oversampling and Hardware Averaging
    3. 4.3 Effect of Sampling Rate on Effective Resolution
    4. 4.4 Influence of the Amplification Factor
  8. 5Summary
  9. 6References

Effect of Sampling Rate on Effective Resolution

The sampling rate of the ADC has significant influence on the effective resolution of the whole signal chain. Defining the effective sampling rate for this evaluation is necessary since the oversampling and averaging features are used in this test. The effective sampling rate is defined by Equation 4.

Equation 4. e f f e c t i v e   s a m p l i n g   r a t e   = n o m i n a l   s a m p l i n g   r a t e a g g r e g a t e d   s a m p l e s  

Figure 4-2 shows the dependency of the effective resolution on the effective sampling rate. This test was executed with the complete signal chain shown in Figure 4-2 but with a constant gain setting of 2 resulting in an internal OPA with a total amplification factor of 100.

Figure 4-2 demonstrates that the effective resolution becomes higher as the sampling rate lowers. Figure 4-2 results in 12.88 bits at an effective sampling rate of 1.8 kSPS. Increasing the effective sampling rate up to 62.5 kSPS results in the effective resolution for this configuration remaining at 11.14 bits.

GUID-20231101-SS0I-WRRL-X9RK-CL1VLGRXKDT5-low.svg Figure 4-2 Effective Resolution vs the Effective Sampling Rate [kSPS]