SLAAEK4 January 2024 MSPM0C1104
For MSPM0, some timer modules have a shadow load and shadow compare register feature which gives the user the flexibility of holding the update of load and CC values until a certain event occurs. This is useful in timing-critical applications where PWM control signals need to be updated with correct timings, such as duty cycle updates.
To control PWM with shadow load / compare, TIMA or specific TIMG are required. The following is the key feature for the use case.