SLAAEM7 September 2024 TAS2120 , TAS2320
The TAS2120 supports edge-rate control to minimize EMI, however the system designer can include passive EMI filter on the Class-D outputs if desired.
When using an EMI filter on the OUT_P or OUT_N pins, the following must be accounted for: