SLAS564H August 2007 – July 2024 CDCE937 , CDCEL937
PRODUCTION DATA
Figure 7-3 shows how the CDCEx937 clock synthesizer is connected to the SDA/SCL serial interface bus. Multiple devices can be connected to the bus but the speed can require reduction (400 kHz is the maximum) if many devices are connected.
Note that the pullup resistors (RP)
depends on the supply voltage, bus capacitance, and number of connected devices. The
recommended pullup value is 4.7 kΩ. The pullup value must meet the minimum sink
current of 3 mA at
VOLmax = 0.4 V for the
output stages (for more details, see SMBus or I2C Bus specification).