SLAS831D March 2014 – March 2018 PCM1860 , PCM1861 , PCM1862 , PCM1863 , PCM1864 , PCM1865
PRODUCTION DATA.
I2C control is selected by the MD0 pin; in this example, MDO is pulled down to ground, so that the device acts as an I2C slave. One address line is supported to select between two devices on the same bus. The I2C control interface is shown in Figure 57.