SLASEJ4C April 2017 – February 2023 PGA460
PRODUCTION DATA
The PGA460 device has a programmable frequency for the burst and number of pulse by configuring the FREQ and P1_PULSE/P2_PULSE registers.
Use Equation 1 to calculate the frequency of burst for a range of 30 kHz to 80 kHz (FREQ_SHIFT bit set to 0).
where
The actual driving frequency of the output stage is derived from the core clock frequency using Equation 1 and Equation 2
where
The PULSE_P1 and PULSE_P2 registers can range from 0 to 31. When set to a value of M that is greater than 0, the M pulse pairs are generated on the OUTA and OUTB outputs.