When any of the P1_PULSE or P2_PULSE bits are set to 0, only the OUTA output generates a pulse, while the OUTB output remains in the high-impedance (High-Z) state during this period. This configuration is used to reduce the output voltage when only short distances are required to be detected.
Note:
- For higher frequency support, the device has an option
to shift up the burst frequency range which occurs by setting the
FREQ_SHIFT bit in the CURR_LIM_P1 register. When this bit is set, the
burst frequency is 6 times higher of the burst frequency selected by the
FREQUENCY register. With this bit set, the range of burst frequencies is
from 180 kHz to 480 kHz with a step of approximately 1.2 kHz.
- The maximum dead time setting should be less than or
equal to t / 8 where t is burst period.