SLASET3D April 2019 – January 2024 TAS2563
PRODUCTION DATA
The TAS2563 can check the speaker terminal for an open or short. This can be used to determine if a problem exists with the speaker or trace to the speaker. The entire operation is performed by the TAS2563 and results reported using the IRQZ pin or read over I2C bus on completion. The load diagnostics can be performed using external audio clock or the internal oscillator.
The speaker open and short thresholds are configured using the respective LDG_RES_UT and LDG_RES_LT registers using equation round(Ω/7*2^22). The load diagnostic mode can be run in two ways. First if the device is in Section 7.3.11.2 the load diagnostic mode can be run by setting LDG_MODE high. The diagnostic will be run and the device will return to Section 7.3.11.2. The load diagnostics can also be run before transitioning to Section 7.3.11.4. This is done by setting the MODE register to Section 7.3.11.5. If the load is within the specified range the device will transition to Section 7.3.11.4 otherwise it will transition to Section 7.3.11.2. When the load diagnostics is run it will play a 22 kHz at -35 dBFS for 100 ms and measure the resistance of the speaker trace. The result is averaged over the time specified by the IVSNS_AVG register. The measured speaker impedance can be read from LDS_RES_VAL1 using the equations Impedance = 7*(LD_RES_VAL1)/2^22) Ω.
IVSNS_AVG[1:0] | SETTING |
---|---|
| 5 ms (default) |
| 10 ms |
| 50 ms |
| 100 ms |
LDG_MODE | SETTING |
---|---|
| Load Diagnostic Not Running (default) |
| Run Load Diagnostic |
LDG_CLK | SETTING |
---|---|
| External TDM |
| Internal Oscillator (default) |