SLASF03 December 2021 DAC11001B
PRODUCTION DATA
When the processor is not able to provide a low-jitter source for the LDAC signal, an external low-jitter LDAC source can be used, as shown in Figure 8-10. The processor can take the LDAC signal as an interrupt and trigger the SPI frame synchronously.