SLASF96 April 2024 AFE20408
PRODUCTION DATA
There is no required supply sequence, but be aware that the device stays in the reset state until all supplies reach the power-good threshold. Also, a hardware or software reset to the device is recommended after the supplies reach the power-good threshold, so that the device can initialize in a known state. Following this reset (or any reset event) wait at least 5ms so that the device registers can properly initialize.
In applications where a negative voltage is applied to VSS first, some small negative voltages can be present at other supply pins, such as the VIO and VDD. The negative voltages at the supply pins can exceed the values listed in Section 5.1, but because these voltages are created from intrinsic circuitry, the voltage levels are safe for operation.