SLASF96 April 2024 AFE20408
PRODUCTION DATA
In many applications, the DAC outputs of the device have a capacitive load. When the DAC outputs transition from one output voltage to another, the short-circuit limit protection can be triggered. If the DAC output buffer reaches the short-circuit current limit of the amplifier, significant current is drawn from the output amplifier supply. Equation 15 shows how to calculate the estimated maximum current that is demanded of the supply during the transition.