SLASF96 April 2024 AFE20408
PRODUCTION DATA
The device resets the serial interface if either SCL or SDA are held low for 25ms (typical) between a START and STOP condition. If the device is holding the bus low, the device releases the bus and waits for a START condition. After the bus is released, all previously received frames on the bus are discarded by the device, and any previous commands and acknowledgment requests are ignored. To avoid activating the timeout function, maintain a communication speed of at least 1kHz for the SCL operating frequency. Figure 6-18 shows the logic diagram for the timeout feature, while Figure 6-19 shows the timing diagram.