SLAU131V October 2004 – February 2020
These directives associate portions of an assembly language program with the appropriate sections:
Section 2 discusses these sections in detail.
Example 1 shows how you can use sections directives to associate code and data with the proper sections. This is an output listing; column 1 shows line numbers, and column 2 shows the SPC values. (Each section has its own program counter, or SPC.) When code is first placed in a section, its SPC equals 0. When you resume assembling into a section after other code is assembled, the section's SPC resumes counting as if there had been no intervening code.
The directives in Example 1 perform the following tasks:
.text | initializes words with the values 1, 2, 3, 4, 5, 6, 7, and 8. |
.data | initializes words with the values 9, 10, 11, 12, 13, 14, 15, and 16. |
var_defs | initializes words with the values 17 and 18. |
.bss | reserves 19 bytes. |
xy | reserves 20 bytes. |
The .bss and .usect directives do not end the current section or begin new sections; they reserve the specified amount of space, and then the assembler resumes assembling code or data into the current section.