SLAU131Y October 2004 – June 2021
The following built-in substitution symbol functions enable you to make decisions on the basis of the string value of substitution symbols. These functions always return a value, and they can be used in expressions. Built-in substitution symbol functions are especially useful in conditional assembly expressions. Parameters of these functions are substitution symbols or character-string constants.
In the function definitions shown in Table 7-1, a and b are parameters that represent substitution symbols or character-string constants. The term string refers to the string value of the parameter. The symbol ch represents a character constant.
Function | Return Value |
---|---|
$symlen (a) | Length of string a |
$symcmp (a,b) | < 0 if a < b; 0 if a = b; > 0 if a > b |
$firstch (a,ch) | Index of the first occurrence of character constant ch in string a |
$lastch (a,ch) | Index of the last occurrence of character constant ch in string a |
$isdefed (a) | 1 if string a is defined in the symbol table |
0 if string a is not defined in the symbol table | |
$ismember (a,b) | Top member of list b is assigned to string a |
0 if b is a null string | |
$iscons (a) | 1 if string a is a binary constant |
2 if string a is an octal constant | |
3 if string a is a hexadecimal constant | |
4 if string a is a character constant | |
5 if string a is a decimal constant | |
$isname (a) | 1 if string a is a valid symbol name |
0 if string a is not a valid symbol name | |
$isreg (a)(1) | 1 if string a is a valid predefined register name |
0 if string a is not a valid predefined register name |
The following example shows built-in substitution symbol functions.
.asg label, ADDR ; ADDR = label
.if ($symcmp(ADDR, "label") = 0) ; evaluates to true
MOV #ADDR, R4
.endif
.asg "x,y,z" , list ; list = x,y,z
.if ($ismember(ADDR,list)) ; ADDR = x, list = y,z
SUB #4, R4 ; sub x
.endif