SLAU132V October   2004  â€“ February 2020

 

  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
    5.     6
  2.   7
    1.     8
    2.     9
    3.     10
    4.     11
    5.     12
  3.   13
    1.     14
    2.     15
    3.     16
      1.      17
      2.      18
      3.      19
      4.      20
      5.      21
      6.      22
      7.      23
      8.      24
      9.      25
      10.      26
      11.      27
      12.      28
    4.     29
      1.      30
      2.      31
    5.     32
      1.      33
      2.      34
        1.       35
      3.      36
      4.      37
      5.      38
      6.      39
      7.      40
      8.      41
      9.      42
      10.      43
    6.     44
    7.     45
      1.      46
      2.      47
    8.     48
    9.     49
    10.     50
    11.     51
      1.      52
      2.      53
    12.     54
      1.      55
    13.     56
    14.     57
  4.   58
    1.     59
    2.     60
    3.     61
      1.      62
    4.     63
      1.      64
      2.      65
    5.     66
    6.     67
      1.      68
      2.      69
    7.     70
      1.      71
        1.       72
        2.       73
        3.       74
        4.       75
        5.       76
        6.       77
        7.       78
        8.       79
      2.      80
      3.      81
      4.      82
    8.     83
      1.      84
        1.       85
        2.       86
      2.      87
        1.       88
        2.       89
        3.       90
    9.     91
    10.     92
    11.     93
      1.      94
      2.      95
    12.     96
    13.     97
      1.      98
      2.      99
      3.      100
      4.      101
      5.      102
      6.      103
      7.      104
      8.      105
      9.      106
      10.      107
      11.      108
      12.      109
      13.      110
  5.   111
    1.     112
      1.      113
      2.      114
      3.      115
    2.     116
      1.      117
      2.      118
    3.     119
      1.      120
        1.       121
          1.        122
        2.       123
        3.       124
      2.      125
      3.      126
      4.      127
      5.      128
      6.      129
      7.      130
      8.      131
      9.      132
        1.       133
  6.   134
    1.     135
      1.      136
    2.     137
    3.     138
    4.     139
    5.     140
    6.     141
      1.      142
    7.     143
    8.     144
      1.      145
      2.      146
      3.      147
        1.       148
        2.       149
      4.      150
        1.       151
    9.     152
    10.     153
    11.     154
    12.     155
      1.      156
      2.      157
      3.      158
      4.      159
      5.      160
      6.      161
        1.       162
        2.       163
        3.       164
        4.       165
      7.      166
      8.      167
        1.       168
        2.       169
        3.       170
      9.      171
      10.      172
      11.      173
      12.      174
      13.      175
      14.      176
      15.      177
      16.      178
      17.      179
      18.      180
      19.      181
      20.      182
      21.      183
      22.      184
      23.      185
      24.      186
      25.      187
      26.      188
      27.      189
      28.      190
      29.      191
      30.      192
        1.       193
        2.       194
        3.       195
      31.      196
      32.      197
    13.     198
    14.     199
    15.     200
    16.     201
      1.      202
      2.      203
      3.      204
    17.     205
      1.      206
      2.      207
      3.      208
      4.      209
      5.      210
    18.     211
  7.   212
    1.     213
      1.      214
      2.      215
      3.      216
      4.      217
      5.      218
      6.      219
    2.     220
      1.      221
        1.       222
        2.       223
        3.       224
        4.       225
      2.      226
    3.     227
    4.     228
      1.      229
      2.      230
      3.      231
    5.     232
    6.     233
      1.      234
      2.      235
        1.       236
        2.       237
      3.      238
        1.       239
          1.        240
          2.        241
        2.       242
          1.        243
          2.        244
      4.      245
      5.      246
    7.     247
      1.      248
      2.      249
      3.      250
      4.      251
      5.      252
    8.     253
      1.      254
      2.      255
      3.      256
      4.      257
        1.       258
          1.        259
        2.       260
          1.        261
    9.     262
      1.      263
      2.      264
      3.      265
        1.       266
        2.       267
        3.       268
        4.       269
          1.        270
          2.        271
          3.        272
          4.        273
        5.       274
        6.       275
      4.      276
        1.       277
        2.       278
    10.     279
  8.   280
    1.     281
      1.      282
      2.      283
      3.      284
      4.      285
      5.      286
      6.      287
      7.      288
      8.      289
    2.     290
      1.      291
        1.       292
      2.      293
      3.      294
      4.      295
        1.       296
      5.      297
        1.       298
    3.     299
    4.     300
      1.      301
      2.      302
        1.       303
        2.       304
          1.        305
          2.        306
          3.        307
          4.        308
      3.      309
        1.       310
        2.       311
  9.   312
    1.     313
    2.     314
      1.      315
      2.      316
      3.      317
  10.   318
    1.     319
  11.   320
    1.     321

Predefined Macro Names

The compiler maintains and recognizes the predefined macro names listed in Table 2-31.

Table 2-31 Predefined MSP430 Macro Names

Macro Name Description
__DATE__(1) Expands to the compilation date in the form mmm dd yyyy
__FILE__(1) Expands to the current source filename
__LARGE_CODE_MODEL__ Defined if --code_model=large is specified
__LARGE_DATA_MODEL__ Defined if --data_model=large or −−data_model=restricted is specified
__LINE__(1) Expands to the current line number
__LONG_PTRDIFF_T__ Defined when --data_model=large is specified. Indicates ptrdiff_t is a long.
__MSP430__ Always defined
__MSP430X__ Defined if --silicon_version=mspx is specified
__MSP430X461X__ Defined if --silicon_version=mspx is specified
__PTRDIFF_T_TYPE__ Set to the type of ptrdiff_t. Determined by the --data_model option.
__signed_chars__ Defined if char types are signed by default (--plain_char=signed)
__SIZE_T_TYPE__ Set to the type of size_t. Determined by the --data_model option.
__STDC__(1) Defined to 1 to indicate that compiler conforms to ISO C Standard. See Section 5.1 for exceptions to ISO C conformance.
__STDC_VERSION__ C standard macro.
__STDC_HOSTED__ C standard macro. Always defined to 1.
__STDC_NO_THREADS__ C standard macro. Always defined to 1.
__TI_COMPILER_VERSION__ Defined to a 7-9 digit integer, depending on if X has 1, 2, or 3 digits. The number does not contain a decimal. For example, version 3.2.1 is represented as 3002001. The leading zeros are dropped to prevent the number being interpreted as an octal.
__TI_EABI__ Defined to 1 if the EABI is enabled (see Section 2.13); otherwise, it is undefined.
__TI_GNU_ATTRIBUTE_SUPPORT__ Defined to 1 if GCC extensions are enabled (which is the default)
__TI_STRICT_ANSI_MODE__ Defined to 1 if strict ANSI/ISO mode is enabled (the --strict_ansi option is used); otherwise, it is defined as 0.
__TI_STRICT_FP_MODE__ Defined to 1 if --fp_mode=strict is used (default); otherwise, it is defined as 0.
__TIME__(1) Expands to the compilation time in the form "hh:mm:ss"
__unsigned_chars__ Defined if char types are unsigned by default (default or −− plain_char=unsigned)
__UNSIGNED_LONG_SIZE_T__ Defined when --data_model=large is specified. Indicates size_t is an unsigned long.
_INLINE Expands to 1 if optimization is used (--opt_level or -O option); undefined otherwise.
Specified by the ISO standard

You can use the names listed in Table 2-31 in the same manner as any other defined name. For example,

printf ( "%s %s" , __TIME__ , __DATE__);

translates to a line such as:

printf ("%s %s" , "13:58:17", "Jan 14 1997");