SLAU132Y September 2004 – June 2021
The C standard assumes only one thread of execution, with the only exception being extremely narrow support for signal handlers. The issue of reentrancy is avoided by not allowing you to do much of anything in a signal handler. However, SYS/BIOS applications have multiple threads which need to modify the same global program state, such as the CIO buffer, so reentrancy is a concern.
Part of the problem of reentrancy remains your responsibility, but the run-time-support environment does provide rudimentary support for multi-threaded reentrancy by providing support for critical sections. This implementation does not protect you from reentrancy issues such as calling run-time-support functions from inside interrupts; this remains your responsibility.
The run-time-support environment provides hooks to install critical section primitives. By default, a single-threaded model is assumed, and the critical section primitives are not employed. In a multi-threaded system such as SYS/BIOS, the kernel arranges to install semaphore lock primitive functions in these hooks, which are then called when the run-time-support enters code that needs to be protected by a critical section.
Throughout the run-time-support environment where a global state is accessed, and thus needs to be protected with a critical section, there are calls to the function _lock(). This calls the provided primitive, if installed, and acquires the semaphore before proceeding. Once the critical section is finished, _unlock() is called to release the semaphore.
Usually SYS/BIOS is responsible for creating and installing the primitives, so you do not need to take any action. However, this mechanism can be used in multi-threaded applications that do not use the SYS/BIOS locking mechanism.
You should not define the functions _lock() and _unlock() functions directly; instead, the installation functions are called to instruct the run-time-support environment to use these new primitives:
void _register_lock (void ( *lock)());
void _register_unlock(void (*unlock)());
The arguments to _register_lock() and _register_unlock() should be functions which take no arguments and return no values, and which implement some sort of global semaphore locking:
extern volatile sig_atomic_t *sema = SHARED_SEMAPHORE_LOCATION;
static int sema_depth = 0;
static void my_lock(void)
{
while (ATOMIC_TEST_AND_SET(sema, MY_UNIQUE_ID) != MY_UNIQUE_ID);
sema_depth++;
}
static void my_unlock(void)
{
if (!--sema_depth) ATOMIC_CLEAR(sema);
}
The run-time-support nests calls to _lock(), so the primitives must keep track of the nesting level.