SLAU132Y September 2004 – June 2021
The function add_device allows you to add and use a device. When a device is registered with add_device, the high-level I/O routines can be used for I/O on that device.
You can use a different protocol to communicate with any desired device and install that protocol using add_device; however, the HOST functions should not be modified. The default streams stdin, stdout, and stderr can be remapped to a file on a user-defined device instead of HOST by using freopen() as in Section 8.3.4.1. If the default streams are reopened in this way, the buffering mode will change to _IOFBF (fully buffered). To restore the default buffering behavior, call setvbuf on each reopened file with the appropriate value (_IOLBF for stdin and stdout, _IONBF for stderr).
The default streams stdin, stdout, and stderr can be mapped to a file on a user-defined device instead of HOST by using freopen() as shown in Section 8.3.4.1. Each function must set up and maintain its own data structures as needed. Some function definitions perform no action and should just return.
Use Unique Function Names
The function names open, read, write, close, lseek, rename, and unlink are used by the low-level routines. Use other names for the device-level functions that you write.
Use the low-level function add_device() to add your device to the device_table. The device table is a statically defined array that supports n devices, where n is defined by the macro _NDEVICE found in stdio.h/cstdio.
The first entry in the device table is predefined to be the host device on which the debugger is running. The low-level routine add_device() finds the first empty position in the device table and initializes the device fields with the passed-in arguments. For a complete description, see the add_device function.