The eZ430-Chronos software development tool is a highly integrated, wearable, wireless development system that is based on the CC430F6137. It may be used as a reference platform for watch systems, a personal display for personal area networks, or as a wireless sensor node for remote data collection.
If you have any feedback or questions, support for the MSP430™ microcontrollers and the eZ430-Chronos™ software development tool is provided by the Texas Instruments Product Information Center (PIC) (support.ti.com), the TI E2E Forum (http://e2e.ti.com/support/microcontrollers/msp430/default.aspx), and the eZ430-Chronos wiki (www.ti.com/chronoswiki). Additional device-specific information can be found on the MSP430 website (www.ti.com/msp430).
The primary sources of MSP430 information are the device-specific data sheets and user's guides. The most up-to-date versions of the user's guide documents available at the time of production have been provided on the CD-ROM included with this tool. However, the most current information is found at www.ti.com/msp430.
Information specific to the eZ430-Chronos development tool can be found at www.ti.com/chronos.
MSP430 device and IDE user's guides may be accessed on the included CD-ROM under the user's guides section. The IDE user's guides include detailed information on setting up a project for the MSP430 using Code Composer Studio™ integrated development environment (IDE) (SLAU157) and the IAR Embedded Workbench™ IDE (SLAU138).
eZ430-Chronos-433 and eZ430-Chronos-868 are restricted from use in the USA and Canada due to frequency conflicts.
eZ430-Chronos-915 is restricted from the use in Europe due to frequency conflicts.
It is the user's responsibility to assure this evaluation module is not operated in any other geographical regions that may be restricted.
Operating temperature 0°C to 40°C (32°F to 104°F)
Storage temperature -20°C to 60°C (-4°F to 140°F)