SLAU319AF July 2010 – September 2022
–
No data required. No delay should be given, and any subsequently required data should be sent as the immediate next byte.
AL, AM, AH
Address bytes. The low, middle, and upper bytes, respectively, of an address.
D1 ... Dn
Data bytes 1 through n (Note: n must be 4 less than the BSL buffer size.)
Length
A byte containing a value from 1 to 255 describing the number of bytes to be transmitted or used in a CRC. In the case of multiple length bytes, they are combined together as described to form a larger value describing the number of required bytes.