SLAU319AF July 2010 – September 2022
The following paragraphs describe BSL internal settings and resources. Because the same device can have implemented different BSL versions, it is very important for the BSL communication program to know the settings and resources. Resources could be either device dependent (for example, RX or TX pins) or BSL-version dependent (for example, byte or word access). The following sections describe the possible variations.