SLAU320AJ July 2010 – May 2021
Reference function: EraseFLASH_430Xv2 and EraseFLASH_430Xv2_wo_release
Similar to what is used for flash programming also the erase operation is handled by a executable code loaded into RAM of the target device. The Flash-Erase-Code provided with this document takes the following parameters.
The Flash-Erase-Code can be executed either under JTAG control or in free-running mode. Similar to what is described in Section 2.3.4.2, the JTAG mailbox system is used to retrieve the current execution state of the Flash-Erase-Code in the target device.
Single stepping over a flash memory segment erase operation is not supported. Any attempt might result in corruption of the program counter.