SLAU320AJ July 2010 – May 2021
The TMS Slot is used to switch between states in the TAP Controller state machine (see Section 2.1.2) of the JTAG module of the target device. The following macros are located in the LowLevelFunc header file in the Replicator example project.