SLAU320AJ July 2010 – May 2021
This instruction enables readout of the data on the MAB with the next 16- or 20-bit data access. The MAB value is not changed during the 16- or 20-bit data access; that is, the 16- or 20-bit data sent on TDI with this command is ignored (0 is sent as a default in the provided software).
In several places throughout the example code, the IR_ADDR_CAPTURE instruction is also used to set the CPU to a defined state after accessing the data bus with the IR_DATA_16BIT instruction.