SLAU330B May 2011 – April 2017
Select this option from the main menu to bring up the Clock submenu. Press S2 to return to the previous menu.
NOTE
The User Experience software initializes the real-time clock to 04:30:00 01/01/2011 when powered is applied to the MSP430 MCU.
Digital Clock: Displays an image of a digital watch with the current time and date.
Analog Clock: Displays an image of an analog clock with the current time.
Set Time: Allows the user to set the current time. Use the scroll wheel to change the value of the current selection. Press push-button S1 is used to advance to the next field. The clock changes take affect after the last field is updated.