3 Firmware Update
To update the firmware of the MSP-BSL, the USB BSL of the MSP430F5510 on the MSP-BSL can be used. To update the firmware:
- Download the latest firmware for the MSP-BSL from the BSL tool folder.
- Download and install the MSP430 USB Firmware Upgrade Example. It is part of the MSP430 USB Developers Package.
- Start the MSP430 USB Firmware Upgrade Example. It shows 'No device connected' at this time.
- Before starting the update, the USB BSL of the MSP-BSL must be invoked.
- Disconnect the MSP-BSL from the USB cable.
- Hold the USB BSL button down while connecting the USB cable.
- Alternatively, switch to baud rate 4801 to invoke the BSL on the MSP-BSL.
The BSL is now invoked, and the Firmware Upgrade Example shows 'Found 1 device' (see Figure 4).
- Now the firmware can be updated.
- Click ‘Select Firmware’ and ‘Browse’ to select the TI-TXT firmware image for the MSPBSL.
- Click ‘Upgrade Firmware’.
The image is loaded, and the MSP-BSL restarts automatically. The new firmware is now ready to use (see Figure 5).