SLAU573C November 2015 – October 2019
The MSP-BSL has a built-in 3.3-V power supply for the target board. It can supply up to 150 mA of current. The power is supplied on pin 6 of the BSL connector but can be cut (by opening PWR_E, see Figure 8) if not needed.
NOTE
Cutting the power supply at PWR_E also prevents the onboard pullup resistors (R10, R11) from being pulled high.